Device Enrollment

In the Device Enrollment tab, you can add a device, view the list of enrolled devices, as well as search for enrolled devices. After the device enrollment it is registered and managed in the Edge Management Portal.

Perform the following steps to add a device:

  1. Go to Administration, select Application Registration within App Provisioning. The Applications Configuration page opens.

  2. Select Device Enrollment.

You can also navigate to Device Enrollment tab by performing the following steps:

  1. Navigate to Digital App Center.

  2. Click Add Application to navigate to Application Configuration screen.

  3. Click Device Enrollment.

Search Device

Using the search bar, you can search from the displayed list of enrolled devices or perform the steps to search an enrolled device from the list:

  1. Click on the Search bar.

  2. Enter the Edge Id.

  3. Select the device id displayed.

Add Device

This feature enables you to enroll a new device. Perform the following steps to add a new device:

  1. Click Add Device.

    Add Device screen

  2. Enter a valid GUID in the Edge Id field.

    GUID is generated online.

  3. Select the required Certificate.

  4. Click Create.